No warning if a pin is assigned in more functional groups in the pins tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No warning if a pin is assigned in more functional groups in the pins tool

815 次查看
vijo
Contributor III

Hi,

the pins can be assigned from the Pins or the Peripheral Signals tab.

In the Peripheral Signals tab no warning is signalled, if the pin allready is used in another functional group.

Am I assigning the pins in a wrong way ?

Regards

vijo

0 项奖励
回复
4 回复数

636 次查看
liborukropec
NXP Employee
NXP Employee

Hello Viggo,

first "Pins" and "Peripherals Signals" views do the same - routing pins, each one offers different look to the pins - how they are ordered.

Next, each functional group can route pins/signals the same or different. If the functional group is marked to be "Called from the initialization function", then the different settings is reported as conflict in the Problems view. If the functional group(s) are not "Called from the initialization function", then the conflict is not reported, as the tool does not know how you are calling the functions in the runtime.

Regards,

Libor

0 项奖励
回复

636 次查看
vijo
Contributor III

Hello Libor,

thank you very much for your help.

Clears things up a lot.

How do I close this conversation and mark it as solved?

regards

Viggo

0 项奖励
回复

636 次查看
liborukropec
NXP Employee
NXP Employee

Hello Viggo,

glad to hear it has been cleared. If you are logged on the community, you should see some button/link "Mark as resolved" or something like that. Probably it can be seen only by the author of the thread (I do not see it). Or it can be under "Actions" menu on my reply.

Regards,

Libor

0 项奖励
回复

636 次查看
vijo
Contributor III

Hello Libor,

Yes, when I displays my very first message in the tread, there is a “Mark as assumed answered”

Regards

Viggo

Fra: liborukropec <admin@community.nxp.com>

Sendt: 27. november 2018 14:24

Til: Viggo Jørgensen <VIJO@tarp.dk>

Emne: Re: - Re: No warning if a pin is assigned in more functional groups in the pins tool

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: No warning if a pin is assigned in more functional groups in the pins tool

reply from Libor Ukropec<https://community.nxp.com/people/liborukropec?et=watches.email.thread> in MCUXpresso Config Tools - View the full discussion<https://community.nxp.com/message/1084767?commentID=1084767&et=watches.email.thread#comment-1084767>

0 项奖励
回复