KV56 pinmuxing not complete in MCUXpresso Config tools V4.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV56 pinmuxing not complete in MCUXpresso Config tools V4.1?

535件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

I'm using MKV56F512 in 144LQFP and try to configure the pin muxing in MCUXpresso Config Tools 4.1

How can I configure CAN2 TxD (Pin 87) and CAN2 RxD (Pin 88) for CAN functionality?

There is no option for ALT2 in the pin muxing tool.

However according DS and RM CAN2 is available on these two pins.

Thanks in advance!CAN2.PNG

1 返信

417件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

According to the datasheet:

pastedImage_1.png

KV58 have 3 can modules (CAN0, CAN1, CAN2) and KV56 MCU only have 2 CAN modules (CAN0 and CAN1), so this is not an error with the config tools.

Hope this helps.

Best regards

Jorge Alcala