Hi,
I'm using a LS1021atwr board, with NXP SDK 1.9
Following the documentation, I'm trying to boot Linux from the Flash.
Both build instructions and Ramdisk Deployment from TFTP refer to a
But in my build folder, I only get a fsl-image-full-ls1021atwr-20160321145603.rootfs.tar.gz with is refused by bootm with
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
How can I procude such a gz.u-boot file ?
Best,
Vincent
已解决! 转到解答。
It seems that patching the IMAGE_FSTYPES_qoriq in fsl-image-full.bb to add ext2.gz.u-boot did the trick, I got the file generated. i'll try to flash it. Thanks for the information !
Hi all,
I got this error when i tried to build ext3.gz
ERROR: Error executing a python function in /home/ravi/pga/svn/trunk/software/imx/filesystem/sources/meta-fsl-demos/recipes-fsl/images/fsl-image-multimedia_backup.bb:
The stack trace of python calls that resulted in this exception/failure was:
File: 'do_rootfs', lineno: 17, function: <module>
0013: # generate final images
0014: create_image(d)
0015:
0016:
*** 0017:do_rootfs(d)
0018:
File: 'do_rootfs', lineno: 14, function: do_rootfs
0010: # generate rootfs
0011: create_rootfs(d)
0012:
0013: # generate final images
*** 0014: create_image(d)
0015:
0016:
0017:do_rootfs(d)
0018:
File: '/home/ravi/pga/svn/trunk/software/imx/filesystem/sources/poky/meta/lib/oe/image.py', lineno: 337, function: create_image
0333: execute_pre_post_process(self.d, post_process_cmds)
0334:
0335:
0336:def create_image(d):
*** 0337: Image(d).create()
0338:
0339:if __name__ == "__main__":
0340: """
0341: Image creation can be called independent from bitbake environment.
File: '/home/ravi/pga/svn/trunk/software/imx/filesystem/sources/poky/meta/lib/oe/image.py', lineno: 315, function: create
0311: execute_pre_post_process(self.d, pre_process_cmds)
0312:
0313: self._remove_old_symlinks()
0314:
*** 0315: image_cmd_groups = self._get_imagecmds()
0316:
0317: for image_cmds in image_cmd_groups:
0318: # create the images in parallel
0319: nproc = multiprocessing.cpu_count()
File: '/home/ravi/pga/svn/trunk/software/imx/filesystem/sources/poky/meta/lib/oe/image.py', lineno: 285, function: _get_imagecmds
0281: localdata.setVar('OVERRIDES', '%s:%s' % (type, old_overrides))
0282: bb.data.update_data(localdata)
0283: localdata.setVar('type', type)
0284:
*** 0285: cmds.append("\t" + localdata.getVar("IMAGE_CMD", True))
0286: cmds.append(localdata.expand("\tcd ${DEPLOY_DIR_IMAGE}"))
0287:
0288: if type in cimages:
0289: for ctype in cimages[type]:
Exception: TypeError: cannot concatenate 'str' and 'NoneType' objects
ERROR: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/ravi/pga/svn/trunk/software/imx/filesystem/build_ramdisk/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-multimedia/backup-r0/temp/log.do_rootfs.14668
ERROR: Task 7 (/home/ravi/pga/svn/trunk/software/imx/filesystem/sources/meta-fsl-demos/recipes-fsl/images/fsl-image-multimedia_backup.bb, do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 4686 tasks of which 490 didn't need to be rerun and 1 failed.
No currently running tasks (4686 of 4687)
Summary: 1 task failed:
/home/ravi/pga/svn/trunk/software/imx/filesystem/sources/meta-fsl-demos/recipes-fsl/images/fsl-image-multimedia_backup.bb, do_rootfs
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Has anyone seen this before.
Please reply.
Regards
Manju
Vincent,
Are you using sd card boot? If yes, why don't you use tar.gz image, create a linux partition on the sd card and untar the image?
For "Ramdisk image is corrupt or invalid", make sure the image is not override uImage, when is loaded in RAM.
Adrian
I already successfully started using sd card boot, but since I have issues performing secure boot from sd card, I wanted to boot from ramdisk, and try an "out of the box" secure boot from ramdisk as described in the SDK. So I'm trying to boot from ram disk atm.
Since I'm trying to flash the -full-, the ramdisk is way bigger. I'll try to put the dtb further away. Thank you for the suggestion !
I almost got it. When I flash the file and perform the 'bootm' command, I get (after some computation time)
## Loading init Ramdisk from Legacy Image at 88000000 ...
Image Name: fsl-image-full-ls1021atwr-201605
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 190697971 Bytes = 181.9 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... Bad Data CRC
Ramdisk image is corrupt or invalid
However verification of the kernel is fine. I'll investigate. If you have any suggestions, do not hesitate :smileywink:
Thank you for the suggestion.
With fsl-image-core, I have manage to get fsl-image-core-ls1021atwr.ext2.gz.u-boot.
Should I comment the "IMAGE_FSTYPES_qoriq" in fsl-image-full.bb to test if I get a *-full-* version of ext2.gz.u-boot ?
Could you try to bitbake fsl-image-core, of course with IMAGE_FSTYPES = "tar.gz ext2.gz ext2.gz.u-boot jffs2 ubi" in QorIQ-SDK-V1.9-20151210-yocto\sources\meta-freescale\recipes-fsl\images\?
Adrian
Go to QorIQ-SDK-V1.9-20151210-yocto\sources\meta-freescale\recipes-fsl\images\ and add ext2.gz.u-boot into fsl-image-minimal.bb as below:
IMAGE_FSTYPES = "tar.gz ext2.gz ext2.gz.u-boot jffs2 ubi"
Adrian
I tried to add a variable in my local.conf file, and it seems to be ignored:
bitbake -e virtual/kernel | grep ^IMAGE_FSTYPES
IMAGE_FSTYPES="ext2.gz.u-boot tar.bz2 ext3 sdcard"
but I only get a tar.gz file, neigher ext2.gz.u-boot nor .sdcard file
Dear addiyi, this value already contains this exact value. I tried to modify the IMAGE_FSTYPES_qoriq of the fsl-image-full.bb file, but it did not help. Maybe this value is overridden somewhere else ?
Best,
Vincent