One-step clock for IEEE 1588 in QorIQ ls1021a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

One-step clock for IEEE 1588 in QorIQ ls1021a

993件の閲覧回数
stefanager
Contributor I

Does QorIQ ls1021a support IEEE 1588 one-step clocks? I can only find support for two-step clocks. If it is supported, is there any documentation or code available that describe one-step clocks in QorIQ?

ラベル(1)
0 件の賞賛
2 返答(返信)

778件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

LS1021A supports IEEE1588-compliant hardware timestamping, this allows high-precision timestamps. The way, how this hardware timestamping is used in your software to implement IEEE1588 - is up to you (your software designer).


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

778件の閲覧回数
stefanager
Contributor I

Thank you for your answer!

However, my question was whether LS1021A supports one-step timestamping. I know that LS1021A supports two-step timestamping, where a packet is hardware timestamped, and the timestamp is sent in a follow up packet. One-step timestamping is a HW feature (not possible to implement in SW) where the hardware timestamp is inserted into the packet that was timestamped. One-step timestamping is an optional feature of the IEEE1588 specification, although it is required in some of the IEEE1588 profiles.

0 件の賞賛