Issue with Enabling DCU/HDMI on LS1021A Kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with Enabling DCU/HDMI on LS1021A Kernel

2,441 次查看
khandavalli
Contributor I

Hello,

I'm working on LayerScape LS1021ATWR facing difficulties in enabling the DCU/HDMI on the LS1 kernel.  Following is my configuration info

SDK: v1.7

Kernel: v3.12.19

U-boot: Bank0: Normal u-boot

             Bank1: Lpuart u-boot

RCW: Bank0: RSR_PPS_70/rcw_1000.bin

           Bank1: rcw_1000_dcu.bin

Switch Settings: SW2: 10000111

                           SW3: 01101001

Jumper Settings: J19-20: 1-2

Filesystem: Graphical image

bootargs=console=ttyLP0,115200 hdmi root=/dev/nfs nfspath=<path to rootfs> rootwait rw ip=dhcp video="fslfb:640x480-32@60,monitor=hdmi"

I'm  trying to boot the kernel from the bank1 where in u-boot is configured for lpuart and rcw is also for dcu (I have also verified with rcw_1000_lpuart.bin in bank1). Im booting via NFS, since booting via sdcard while testing hangs the board. I wanted to know if i'm missing something in the bootargs, I have verified that all the modules required for dcu are compiled built-in and required dts information is also present. could you please help in enabling the HDMI in kernel while booting from bank1.

Regards,

Arun Khandavalli.

标签 (1)
0 项奖励
3 回复数

1,410 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello khandavalli,

First please check whether u-boot can be displayed with HDMI.

=> setenv video-mode "fslfb:640x480-32@60,monitor=hdmi"

=> save

=> reset

build kernel images with enable below kernel option:

Device Drivers --->
    < > Multimedia support ----
        Graphics support --->
            <*> Support for frame buffer devices  --->
                <*> Si Image SII9022 DVI/HDMI Interface Chip
                <*> Freescale DCU framebuffer support
                    Console display driver support --->
                        <*> Framebuffer Console support
                        [*] Map the console to the primary display device
                        [*] Framebuffer Console Rotation
                [*] Bootup logo --->
                    --- Bootup logo
                    [*] Standard black and white Linux logo
                    [*] Standard 16-color Linux logo
                    [*] Standard 224-color Linux logo
    < > Sound card support ----

set bootargs in uboot:

setenv console 'ttyLP0,115200 hdmi res=640x480'

boot up kernel then kill terminal and restart terminal

root@ls1021atwr:~# killall matchbox-window-manager

root@ls1021atwr:~# xinit /etc/X11/Xsession

Please let me know, if your problem remain.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,410 次查看
khandavalli
Contributor I

Hello Yiping,

At the u-boot level with lpuart and rcw-dcu in bank1 im able to get the hdmi display in the u-boot with 640x480 resolution.

My problem is during the kernel booting, all the related kernel configuration parameters I have enabled:

1) CONFIG_ FB_FSL_SII902X = y

2)  CONFIG_FB_FSL_DCU = y

3) CONFIG_LOGO = y

4) CONFIG_LOGO_LINUX_MONO = y

5) CONFIG_LOGO_LINUX_CL UT224 =y

6) CONFIG_LOGO_LINUX_CLUT224  = y

7) CONFIG_FRAMEBUFFER_CONSOLE = y

I have set the bootargs for booting as suggested:

=> pri bootargs

bootargs=root=/dev/ram rw console=ttyLP0,115200 hdmi res=640x480

Booting Linux on physical CPU 0xf00

Linux version 3.12.19-rt30 (akhandava@ubuntu) (gcc version 4.9.1 (Sourcery CodeBench 2014.11-46) ) #1 SMP Thu May 28 13:33:57 IST 2015

CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=70c73c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale LS1021A, model: LS1021A TWR Board

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 9 pages/cpu @80e44000 s12544 r8192 d16128 u36864

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

Kernel command line: root=/dev/ram rw console=ttyLP0,115200 hdmi res=640x480

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 988112K/1048576K available (3531K kernel code, 331K rwdata, 1840K rodata, 232K init, 390K bss, 60464K reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f800000 - 0x7fe00000   (   6 MB)

      .text : 0x80008000 - 0x80546f2c   (5372 kB)

      .init : 0x80547000 - 0x80581100   ( 233 kB)

      .data : 0x80582000 - 0x805d4ee8   ( 332 kB)

       .bss : 0x805d4ee8 - 0x806369b4   ( 391 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1

Hierarchical RCU implementation.

        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

NR_IRQS:16 nr_irqs:16 16

Architected cp15 timer(s) running at 12.50MHz (phys).

Switching to timer-based delay loop

sched_clock: ARM arch timer >56 bits at 12500kHz, resolution 80ns

sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 25.00 BogoMIPS (lpj=125000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: update cpu_power 1024

CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00

Setting up static identity map for 0x8034e208 - 0x8034e26c

CPU1: Booted secondary processor

CPU1: update cpu_power 1024

CPU1: thread -1, cpu 1, socket 15, mpidr 80000f01

Brought up 2 CPUs

SMP: Total of 2 processors activated.

CPU: All CPU(s) started in HYP mode.

CPU: Virtualization extensions available.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

syscon 1570000.scfg: regmap [mem 0x01570000-0x0157ffff] registered

irq: no irq domain found for /soc/uqe@2400000/qeic@80 !

irq: no irq domain found for /soc/uqe@2400000/qeic@80 !

hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 8 bytes.

bio: create slab <bio-0> at 0

3P3V: 3300 mV

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

i2c i2c-2: of_i2c: modalias failure on /soc/i2c@21a0000/ltc2945@67

i2c i2c-2: IMX I2C adapter registered

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource arch_sys_counter

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 44948K (bc349000 - bef2e000)

hw perfevents: enabled with ARMv7 Cortex-A7 PMU driver, 5 counters available

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

squashfs: version 4.0 (2009/01/31) Phillip Lougher

Registering unionfs 2.6 (for 3.12.26)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 2017

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

layerscape-pcie 3400000.pcie: phy link never came up

layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x1000-0xffff]

pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])

pci_bus 0000:00: root bus resource [bus 00-ff]

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0000:00:00.0: BAR 1: assigned [mem 0x4040000000-0x4043ffffff]

pci 0000:00:00.0: BAR 0: assigned [mem 0x4044000000-0x4044ffffff]

pci 0000:00:00.0: BAR 6: assigned [mem 0x4045000000-0x4045ffffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01]

layerscape-pcie 3500000.pcie: phy link never came up

layerscape-pcie 3500000.pcie: PCI host bridge to bus 0001:00

pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x0000-0xffff])

pci_bus 0001:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])

pci_bus 0001:00: root bus resource [bus 00-ff]

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0001:00:00.0: BAR 1: assigned [mem 0x4840000000-0x4843ffffff]

pci 0001:00:00.0: BAR 0: assigned [mem 0x4844000000-0x4844ffffff]

pci 0001:00:00.0: BAR 6: assigned [mem 0x4845000000-0x4845ffffff pref]

pci 0001:00:00.0: PCI bridge to [bus 01]

Sii902x: read id = 0xB0

-0x02-0x03

-0x00

Unimplemented SVD code 2

Unimplemented SVD code 22

Unimplemented SVD code 31

syscon 1570000.scfg: Failed to create debugfs directory

Console: switching to colour frame buffer device 60x34

fb0: fb device registered successfully.

fb1: fb device registered successfully.

fb2: fb device registered successfully.

fb3: fb device registered successfully.

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

of_serial: probe of 21c0500.serial failed with error -22

of_serial: probe of 21c0600.serial failed with error -22

of_serial 2402200.ucc: clk or clock-frequency not defined

of_serial: probe of 2402200.ucc failed with error -2

serial: Freescale lpuart driver

2950000.serial: ttyLP0 at MMIO 0x2950000 (irq = 112, base_baud = 6250000) is a FSL_LPUART

console [ttyLP0] enabled

brd: module loaded

loop: module loaded

Unimplemented SVD code 2

60000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e

Amd/Fujitsu Extended Query Table at 0x0040

  Amd/Fujitsu Extended Query version 1.3.

number of CFI chips: 1

Unimplemented SVD code 22

Unimplemented SVD code 31

8 ofpart partitions found on MTD device 60000000.nor

Creating 8 MTD partitions on "60000000.nor":

0x000000000000-0x000000020000 : "NOR bank0 RCW Image"

0x000000020000-0x000000120000 : "NOR DTB Image"

0x000000120000-0x000000920000 : "NOR Linux Kernel Image"

0x000000920000-0x000003f20000 : "NOR Ramdisk Root File System Image"

0x000003f80000-0x000004000000 : "NOR bank4 u-boot Image"

0x000004000000-0x000004020000 : "NOR bank4 RCW Image"

0x000004020000-0x000007f20000 : "NOR JFFS2 ROOT File System Image"

0x000007f80000-0x000008000000 : "NOR bank0 u-boot Image"

fsl-quadspi 1550000.quadspi: found mr25h256, expected n25q128a13

fsl-quadspi 1550000.quadspi: mr25h256 (32 Kbytes)

fsl-quadspi 1550000.quadspi: Unsupported cmd 0x03

fsl-quadspi 1550000.quadspi: QuadSPI SPI NOR flash driver

CAN device driver interface

libphy: Freescale PowerQUICC MII Bus: probed

fsl-gianfar ethernet.4: enabled errata workarounds, flags: 0x4

fsl-gianfar ethernet.4 eth0: mac: 00:04:9f:03:63:bf

fsl-gianfar ethernet.4 eth0: Running with NAPI enabled

fsl-gianfar ethernet.4 eth0: RX BD ring size for Q[0]: 256

fsl-gianfar ethernet.4 eth0: TX BD ring size for Q[0]: 256

fsl-gianfar ethernet.5: enabled errata workarounds, flags: 0x4

fsl-gianfar ethernet.5 eth1: mac: 00:04:9f:03:63:bf

fsl-gianfar ethernet.5 eth1: Running with NAPI enabled

fsl-gianfar ethernet.5 eth1: RX BD ring size for Q[0]: 256

fsl-gianfar ethernet.5 eth1: TX BD ring size for Q[0]: 256

fsl-gianfar ethernet.6: enabled errata workarounds, flags: 0x4

fsl-gianfar ethernet.6 eth2: mac: 00:04:9f:03:63:c0

fsl-gianfar ethernet.6 eth2: Running with NAPI enabled

fsl-gianfar ethernet.6 eth2: RX BD ring size for Q[0]: 256

fsl-gianfar ethernet.6 eth2: TX BD ring size for Q[0]: 256

e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k

e1000e: Copyright(c) 1999 - 2013 Intel Corporation.

xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1

xhci-hcd xhci-hcd.0.auto: irq 125, io mem 0x03100000

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usbcore: registered new interface driver usb-storage

mousedev: PS/2 mouse device common for all mice

i2c /dev entries driver

imx2-wdt 2ad0000.wdog: timeout 60 sec (nowayout=0)

qoriq_cpufreq: Freescale PowerPC qoriq CPU frequency scaling driver

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: no vqmmc regulator found

mmc0: no vmmc regulator found

mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA

caam 1700000.crypto: Entropy delay = 3200

caam 1700000.crypto: Instantiated RNG4 SH0

caam 1700000.crypto: Instantiated RNG4 SH1

caam 1700000.crypto: device ID = 0x0a14030000000000 (Era 67108864)

caam 1700000.crypto: job rings = 4, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 1710000.jr: registering rng-caam

caam 1700000.crypto: fsl,sec-v5.3 algorithms registered in /proc/crypto

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

sgtl5000 1-000a: sgtl5000 revision 0x11

sgtl5000 1-000a: Failed to get supply 'VDDD': -19

1-000a: 1200 mV normal

sgtl5000 1-000a: Using internal LDO instead of VDDD

vf610-sgtl5000 sound.9:  sgtl5000 <-> 2b50000.sai mapping ok

oprofile: using timer interrupt.

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

Key type dns_resolver registered

regulator-dummy: disabling

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

ALSA device list:

  #0: FSL-VF610-TWR-BOARD

usb 1-1: new high-speed USB device number 2 using xhci-hcd

RAMDISK: gzip image found at block 0

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 4 ports detected

usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd

usb 2-1: Parent hub missing LPM exit latency info.  Power management will be impacted.

hub 2-1:1.0: USB hub found

hub 2-1:1.0: 4 ports detected

VFS: Mounted root (ext2 filesystem) on device 1:0.

devtmpfs: mounted

Freeing unused kernel memory: 232K (80547000 - 80581000)

Starting udevboo

udevd[131]: starting version 182

Starting Bootlog daemon: bootlogd.

Populating dev cache

Configuring network interfaces... udhcpc (v1.21.1) started

Sending discover...

libphy: mdio@2d24000:02 - Link is Down

Sending discover...

Sending discover...

No lease, failing

Starting rpcbind daemon...rpcbind: cannot create socket for udp6

rpcbind: cannot create socket for tcp6

done.

hwclock: can't open '/dev/misc/rtc': No such file or directory

Mon Oct 27 02:02:00 UTC 2014

hwclock: can't open '/dev/misc/rtc': No such file or directory

Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...

update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)

Removing any system startup links for run-postinsts ...

  /etc/rcS.d/S99run-postinsts

INIT: Entering runlevel: 5

Starting system message bus: dbus.

Starting OpenBSD Secure Shell server: sshd

  generating ssh RSA key...

  generating ssh ECDSA key...

  generating ssh DSA key...

done.

Starting Xserver

hwclock: can't open '/dev/misc/rtc': No such file or directory

creating NFS state directory: _XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6

_XSERVTransOpen: transport open failed for inet6/ls1021atwr:0

_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6

X.Org X Server 1.14.0

Release Date: 2013-03-05

X Protocol Version 11, Revision 0

Build Operavgaarb: this pci device is not a vga device

ting System: Linux 2.6.32-431.el6.x86_64 x86_64

Current Operating System: Linux ls1021atwr 3.12.19-rt30 #1 SMP Thu May 28 13:33:57 IST 2015 armv7l

Kvgaarb: this pci device is not a vga device

ernel command line: root=/dev/ram rw console=ttyLP0,115200 hdmi res=640x480

Build Date: 24 October 2014  07:38:18PM

Current version of pixman: 0.30.2

        Before reporting problems, check http://wiki.x.org

        to make sure that you have the latest version.

Markers: (--) probed, (**) from config file, (==) default setting,

        (++) from command line, (!!) notice, (II) informational,

        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.

(==) Log file: "/var/log/Xorg.0.log", Time: Mon Oct 27 02:02:07 2014

(==) Using system config directory "/usr/share/X11/xorg.conf.d"

done

starting 8 nfsd kernel threads: Initializing built-in extension Generic Event Extension

Initializing built-in extension SHAPE

Initializing built-in extension MIT-SHM

Initializing built-in extension XInputExtension

Initializing built-in extension XTEST

Initializing built-in extension BIG-REQUESTS

Initializing built-in extension SYNC

Initializing built-in extension XKEYBOARD

Initializing built-in extension XC-MISC

Initializing built-in extension XFIXES

Initializing built-in extension RENDER

Initializing built-in extension RANDR

Initializing built-in extension COMPOSITE

Initializing built-in extension DAMAGE

Initializing built-in extension MIT-SCREEN-SAVER

Initializing built-in extension DOUBLE-BUFFER

Initializing built-in extension DPMS

Initializing built-in extension X-Resource

Initializing built-in extension XVideo

Initializing built-in extension XVideo-MotionCompensation

Initializing built-in extension XFree86-VidModeExtension

Initializing built-in extension XFree86-DGA

Initializing built-in extension XFree86-DRI

Initializing built-in extension DRI2

rpc.nfsd: Unable to access /proc/fs/nfsd errno 2 (No such file or directory).

Please try, as root, 'mount -t nfsd nfsd /proc/fs/nfsd' and then restart rpc.nfsd to correct the problem

done

starting mountd: done

starting statd: done

Starting syslogd/klogd: done

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

   ...done.

Starting Telephony daemon

Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.5 ls1021atwr /dev/ttyLP0

ls1021atwr login: D-BUS per-session daemon address is: unix:abstract=/tmp/dbus-sILIX0MLt1,guid=149ad50a6835233f44479c28544da7a0

Size 1024x768 not found in available modes

matchbox: Cant find a keycode for keysym 269025056

matchbox: ignoring key shortcut XF86Calendar=!$contacts

matchbox: Cant find a keycode for keysym 2809

matchbox: ignoring key shortcut telephone=!$dates

matchbox: Cant find a keycode for keysym 269025050

matchbox: ignoring key shortcut XF86Start=!matchbox-remote -desktop

Poky (Yocto Project Reference Distro) 1.5 ls1021atwr /dev/ttyLP0

ls1021atwr login:

Poky (Yocto Project Reference Distro) 1.5 ls1021atwr /dev/ttyLP0

I have following points to add:

1) SII9022 DVI/HDMI Interface Chip has got successfully probed, it is reading the EDID and we can see the prints from the driver in the kernel log.

2) I have seen some warning messages from fbcore "Unimplemented SVD " which when i digged through the code seem related to the CESA. Does these warning effect the functionality of the HDMI?

3) I have also seen few waning/errors from the matchbox:

matchbox: Cant find a keycode for keysym 269025056

matchbox: ignoring key shortcut XF86Calendar=!$contacts

matchbox: Cant find a keycode for keysym 2809

matchbox: ignoring key shortcut telephone=!$dates

Is there anything to be added inthe bootargs or enabled in the kernel defconfig?

0 项奖励

1,410 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Reply to khandavalli,

It seems that he message "Unimplemented SVD" is abnormal, we never see it.

The following Kernel boot bootargs is used.

root=/dev/ram0 rw console=ttyLP0,115200 hdmi

The following options are enabled.

CONFIG_ FB_FSL_SII902X

CONFIG_FB_FSL_DCU

CONFIG_LOGO

CONFIG_LOGO_LINUX_MONO

CONFIG_LOGO_LINUX_VGA16

CONFIG_LOGO_LINUX_CLUT224

CONFIG_FRAMEBUFFER_CONSOLE


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励