How is IFC-TE, IFC_BCTL, and IFC_CLK0 being used in u-boot and the kernel for the IFC?
If IFC_BCTL and IFC_CLK0 for the IFC is removed on a custom board, what are the implications for SDK 2.0 and the LS1043ARDB?
Have a great day,
The u-boot/kernel IFC driver should take into account using IFC_TE pin and sets the TE bit in the Chip-select Property register properly. While used IFC_BCTL signal should be enabled in the Chip-Select Option register.
Unused IFC_BCTL and IFC_CLK0 output signals do not require any u-boot/kernel software modifications.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------