FLEXSPI erase and write issue on 2160A-TCD platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FLEXSPI erase and write issue on 2160A-TCD platform

1,014 次查看
andy_ueng
Contributor I

We encounter FLEXSPI erase and write issue. We use the following commands to test FLEXSPI read, write, and erase.
mtd_debug erase /dev/mtd2 0x0000000 0x10000
dd if=/dev/zero of=data.hex count=1 bs=65536
mtd_debug write /dev/mtd2 0x0000000 0x10000 data.hex
mtd_debug read /dev/mtd2 0x0000000 0x10000 dump

The contents of data.hex and dump files should be same. But unfortunately the contents of these two files are not identical.

P.S.
fsl-lx2160a-tcd.dts is dts file.
spi-nxp-fspi.c is FLEXSPI driver source file.
erase.PNG, read.PNG, and write.PNG are captured from Zeroplus logic analyzer.
Plese kindly give us your advice.
Thanks!

0 项奖励
3 回复数

957 次查看
andy_ueng
Contributor I

I have fixed this issue by disabling erasing and writing protection from NOR flash register.

0 项奖励

991 次查看
andy_ueng
Contributor I
    Thanks for your reply. We use fspi section in fsl-lx2160a-tcd.dts. Do we need to modify the following fspi section?
&fspi {
status = "okay";
 
n25q128a0: flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "jedec,spi-nor";
m25p,fast-read;
spi-max-frequency = <20000000>;
reg = <0>;
spi-rx-bus-width = <4>;
spi-tx-bus-width = <4>;
 
partitions {
compatible = "fixed-partitions";
#address-cells = <1>;
#size-cells = <1>;
 
partition@0 {
label = "BL2";
reg = <0 0x100000>;
};
partition@100000 {
label = "BL3";
reg = <0x100000 0x400000>;
};
partition@500000 {
label = "BootEnv";
reg = <0x500000 0x100000>;
};
partition@600000 {
label = "SecureBoot";
reg = <0x600000 0x200000>;
};
partition@800000 {
label = "DDRPHY";
reg = <0x800000 0x80000>;
};
partition@880000 {
label = "FuseHeader";
reg = <0x880000 0x80000>;
};
partition@900000 {
label = "DPAA1";
reg = <0x900000 0x80000>;
};
partition@980000 {
label = "ETHPHY";
reg = <0x980000 0x80000>;
};
partition@A00000 {
label = "DPAA2";
reg = <0xA00000 0x300000>;
};
partition@D00000 {
label = "DPAA2DPL";
reg = <0xD00000 0x100000>;
};
partition@E00000 {
label = "DPAA2DPC";
reg = <0xE00000 0x100000>;
};
partition@F00000 {
label = "DTB";
reg = <0xF00000 0x100000>;
};
};
};
 
The following URL is datasheet of NOR flash we use.
0 项奖励

998 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In your dts file, please define FSPI flash device and configure "compatible" property according to the flash device on your target board. Please refer to the following example, please refer to SPI NOR flash driver drivers/mtd/spi-nor/spi-nor.c.

&fspi {
status = "okay";

mt35xu512aba0: flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "spansion,m25p80";
m25p,fast-read;
spi-max-frequency = <50000000>;
reg = <0>;
spi-rx-bus-width = <8>;
spi-tx-bus-width = <8>;
};

mt35xu512aba1: flash@1 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "spansion,m25p80";
m25p,fast-read;
spi-max-frequency = <50000000>;
reg = <1>;
spi-rx-bus-width = <8>;
spi-tx-bus-width = <8>;
};
};

0 项奖励