Building UEFI-sd boot for the LX2160A.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building UEFI-sd boot for the LX2160A.

1,838 Views
pieter_jansenvv
Contributor I

Building a UEFI on SD firmware image for the LX2160 using flex-builder, as follows:
flex-builder -i mkfw -m lx2160ardb -b sd -B uefi

results in:
uefi_sdboot is not supported

From the Layerscape SDK user guide (Section 5.4.5) it seems possible to build a uefi bootloader.

This unfortunately leads to the following on boot:
add-symbol-file /packages/firmware/uefi/Build/LX2160aRdbPkg/DEBUG_GCC49/AARCH64/Silicon/NXP/Drivers/DtPlatformDxe/DtPlatformDxe/DEBUG/DtPlatformDxe.dll 0xF9D3E000

Loading driver at 0x000F9D3D000 EntryPoint=0x000F9D3E048 DtPlatformDxe.efi

InstallProtocolInterface: BC62157E-3E33-4FEC-9920-2D3B36D750DF F929CC18

ProtectUefiImageCommon - 0xF9297040

- 0x00000000F9D3D000 - 0x0000000000010000

SetUefiImageMemoryAttributes - 0x00000000F9D3D000 - 0x0000000000001000 (0x0000000000004008)

SetUefiImageMemoryAttributes - 0x00000000F9D3E000 - 0x000000000000D000 (0x0000000000020008)

SetUefiImageMemoryAttributes - 0x00000000F9D4B000 - 0x0000000000002000 (0x0000000000004008)

Synchronous Exception at 0x00000000F9D42694

Is this a known issue and is there a throughout guide on how to build UEFI sdboot for the LX2160?

I appreciate any feedback.

0 Kudos
Reply
1 Reply

1,590 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Pieter Jansen van Vuuren,

UEFI SD boot is not supported on LX2160, you could use UEFI xspi boot, please generate the firmware image with the following command.

$ flex-builder -i mkfw -m lx2160ardb -b xspi -B uefi

Thanks,

Yiping

0 Kudos
Reply