Modify LS1046ARDB MAC6 from non-Fixed to Fixed Link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Modify LS1046ARDB MAC6 from non-Fixed to Fixed Link

Modify LS1046ARDB MAC6 from non-Fixed to Fixed Link

On the LS1046ARDB, there are 2 1G SGMII with PHY, but sometimes customer want to get PHY-less connection to evaluate the performance, so they may have to change the non-fixed link properties into fixed-link by reconfiguration the SW configuration.

In this document, it will give details of configuring the LS1046ARDB to support the fixed-link requirement with LSDK2108 focus on the DTS and Linux kernel. The ethernet MAC in this document is FM1 mEMAC6: 1AE_A000h. Because there is no PHY-less connection on board. We only provide the status when the MAC has been configured.

附件
无评分
版本历史
最后更新:
‎11-05-2023 08:10 PM
更新人: