Warning to LPC811 and 812 users.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Warning to LPC811 and 812 users.

227 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ppx on Fri Feb 14 06:13:57 MST 2014
Just downloaded V1.3 of the user manual and found this in changes!

Changed the ISP entry pin from PIO0_1 to PIO0_12 for TSSOP and SOP packages.
0 Kudos
Reply
1 Reply

215 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ppx on Tue Feb 25 02:36:46 MST 2014
Small comment. This is only for version 4C and newer. Older versions still use PIO-0-0. Version are the end of the last line on the chip marking. I find it incredible that they can change pin numbers in the middle of production and rendering several customers with unusable PCBs.
0 Kudos
Reply