Content originally posted in LPCWare by petermeter69 on Fri Feb 28 07:41:58 MST 2014
Hello,
I am new to LpcXpresso, sorry if this is a basic question!
I have installed LPCXpresso v6.1.4 [Build 194] [2014-01-15].
I have loaded the example projects of the base board.
I cannot load them onto an any LPCXPresso boards (I have two of them: LPC1227, LPC1769) because of following error:
Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_lpc11_13_nxp -msg-port=2538 -g -mi -2 -pLPC1227/301 -vendor=NXP -vc -e0 -wire=winUSB -flash-driver=LPC11_12_13_128K_8K.cfx
Error message from debugger back end:
Remote communication error. Target disconnected.: No error.
Remote communication error. Target disconnected.: No error.
02: Failed on connect
02: Failed on connect
Bad ACK returned from status - wire error.
Emu(0): Connected. Was: None. DpID: EDB6. Info: WIN64HS12
I have tried it with board on extra powered base board, separated (alone standing) board, and LPCLink + other board over JTAG interface, without any success.
Could somebody please point me towards a solution to this?
Peter