11u24 failed to connect - MEM-AP is not selected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

11u24 failed to connect - MEM-AP is not selected

243件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Thu Feb 20 17:14:14 MST 2014
I have a 11U24 dev board (OM13014) and uploaded different examples from the the sample collection lpcopen_v2_00a_lpcxpresso_nxp_lpcxpresso_11u14.zip successfully, using lpcxpresso 6.1.4_194 on Fedora 19.

I loaded the sample 'nxp_lpcxpresso_11u14_periph_pinint' and now I am stuck uploading
any kind of sample project. Even those that worked before are not uploading anylonger.

I get the following error:

  0.2: failed to connect
  MEM-AP is not selected
  Emu(0): Conn&Reset. Was: None. DpID: BB114744.

I tried switch the board to ISP mode manually, but no success so far.
Any idea what to do next?
0 件の賞賛
1 返信

229件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Tue Feb 25 15:18:14 MST 2014
to be continued here:

http://www.lpcware.com/content/forum/11u24-bricked
0 件の賞賛