USB HID Keyboard LPC1754

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB HID Keyboard LPC1754

1,539件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maxxracing on Fri Dec 04 06:35:51 MST 2015
Hello,

I would like to make a USB HID Keyboard with my LPC1754.

I have already a program with the LPC1754 with a usb hid, but i on the PC side i have a software that make a HID connection and after that a make transactions.

I would like that my board be recognised by the PC like a hid keyboard, and the datas send to the PC will be write on the active cursor like a hid keyboard.

I already modify HID_ReportDescriptor[] in the file usbdesc.c, the PC recognised the board like a keyboard PIH, so i think it's a good start.
But after that i can't send data to the PC.

I have in the file usbuser.c this callback, but since i modify HID_ReportDescriptor, it's not tell:
/*
*  USB Endpoint 1 Event Callback
*   Called automatically on USB Endpoint 1 Event
*    Parameter:       event
*/

void USB_EndPoint1 (uint32_t event) {

  switch (event) {
    case USB_EVT_IN:
      GetInReport();
      USB_WriteEP(HID_EP_IN, &InReport, sizeof(InReport));

      break;
  }
}

file usbdesc.c :

const uint8_t HID_ReportDescriptor[] = {
/****/ 0x05, 0x01,     /* USAGE_PAGE (Generic Desktop) */
/****/ 0x09, 0x06,     /* USAGE (Keyboard) */
/****/ 0xa1, 0x01,     /* COLLECTION (Application) */
/******/ 0x05, 0x07,   /*   USAGE_PAGE (Keyboard) */
/******/ 0x85, 0x01,   /*   REPORT_ID (1) */
  /* Ctrl, Shift and other modifier keys, 8 in total */
/******/ 0x19, 0xe0,   /*   USAGE_MINIMUM (kbd LeftControl) */
/******/ 0x29, 0xe7,   /*   USAGE_MAXIMUM (kbd Right GUI) */
/******/ 0x15, 0x00,   /*   LOGICAL_MINIMUM (0) */
/******/ 0x25, 0x01,   /*   LOGICAL_MAXIMUM (1) */
/******/ 0x75, 0x01,   /*   REPORT_SIZE (1) */
/******/ 0x95, 0x08,   /*   REPORT_COUNT (8) */
/******/ 0x81, 0x02,   /*   INPUT (Data,Var,Abs) */
/* Reserved byte */
/******/ 0x95, 0x01,   /*   REPORT_COUNT (1) */
  /******/ 0x75, 0x08,   /*   REPORT_SIZE (8) */
/******/ 0x81, 0x01,   /*   INPUT (Cnst,Ary,Abs) */
/* LEDs for num lock etc */
/******/ 0x95, 0x05,   /*   REPORT_COUNT (5) */
/******/ 0x75, 0x01,   /*   REPORT_SIZE (1) */
/******/ 0x05, 0x08,   /*   USAGE_PAGE (LEDs) */
/******/ 0x85, 0x01,   /*   REPORT_ID (1) */
/******/ 0x19, 0x01,   /*   USAGE_MINIMUM (Num Lock) */
/******/ 0x29, 0x05,   /*   USAGE_MAXIMUM (Kana) */
/******/ 0x91, 0x02,   /*   OUTPUT (Data,Var,Abs) */
  /* Reserved 3 bits */
/******/ 0x95, 0x01,   /*   REPORT_COUNT (1) */
/******/ 0x75, 0x03,   /*   REPORT_SIZE (3) */
/******/ 0x91, 0x03,   /*   OUTPUT (Cnst,Var,Abs) */
/* Slots for 6 keys that can be pressed down at the same time */
/******/ 0x95, 0x06,   /*   REPORT_COUNT (6) */
/******/ 0x75, 0x08,   /*   REPORT_SIZE (8) */
/******/ 0x15, 0x00,   /*   LOGICAL_MINIMUM (0) */
/******/ 0x25, 0x65,   /*   LOGICAL_MAXIMUM (101) */
  /******/ 0x05, 0x07,   /*   USAGE_PAGE (Keyboard) */
/******/ 0x19, 0x00,   /*   USAGE_MINIMUM (Reserved (no event indicated)) */
/******/ 0x29, 0x65,   /*   USAGE_MAXIMUM (Keyboard Application) */
/******/ 0x81, 0x00,   /*   INPUT (Data,Ary,Abs) */
/****/ 0xc0,                 // END_COLLECTION
};

/* USB Standard Device Descriptor */
const uint8_t USB_DeviceDescriptor[] = {
  USB_DEVICE_DESC_SIZE,              /* bLength */
  USB_DEVICE_DESCRIPTOR_TYPE,        /* bDescriptorType */
  WBVAL(0x0200), /* 2.00 */          /* bcdUSB */
  0x00,                              /* bDeviceClass */
  0x00,                              /* bDeviceSubClass */
  0x00,                              /* bDeviceProtocol */
  USB_MAX_PACKET0,                   /* bMaxPacketSize0 */
  WBVAL(0x1FC9),                     /* idVendor */
  WBVAL(0x8002),                     /* idProduct */
  WBVAL(0x0100), /* 1.00 */          /* bcdDevice */
  0x01,                              /* iManufacturer */
  0x02,                              /* iProduct */
  0x03,                              /* iSerialNumber */
  0x01                               /* bNumConfigurations: one possible configuration*/
};


/* USB Configuration Descriptor */
/*   All Descriptors (Configuration, Interface, Endpoint, Class, Vendor) */
const uint8_t USB_ConfigDescriptor[] = {
/* Configuration 1 */
  USB_CONFIGUARTION_DESC_SIZE,       /* bLength */
  USB_CONFIGURATION_DESCRIPTOR_TYPE, /* bDescriptorType */
  WBVAL(                             /* wTotalLength */
    USB_CONFIGUARTION_DESC_SIZE +
    USB_INTERFACE_DESC_SIZE     +
    HID_DESC_SIZE               +
    USB_ENDPOINT_DESC_SIZE
  ),
  0x01,                              /* bNumInterfaces */
  0x01,                              /* bConfigurationValue */
  0x00,                              /* iConfiguration */
  USB_CONFIG_BUS_POWERED /*|*/       /* bmAttributes */
/*USB_CONFIG_REMOTE_WAKEUP*/,
  USB_CONFIG_POWER_MA(100),          /* bMaxPower */
/* Interface 0, Alternate Setting 0, HID Class */
  USB_INTERFACE_DESC_SIZE,           /* bLength */
  USB_INTERFACE_DESCRIPTOR_TYPE,     /* bDescriptorType */
  0x00,                              /* bInterfaceNumber */
  0x00,                              /* bAlternateSetting */
  0x01,                              /* bNumEndpoints */
  USB_DEVICE_CLASS_HUMAN_INTERFACE,  /* bInterfaceClass */
  HID_SUBCLASS_NONE,                 /* bInterfaceSubClass */
  HID_PROTOCOL_NONE,                 /* bInterfaceProtocol */
  0x04,                              /* iInterface */
/* HID Class Descriptor */
/* HID_DESC_OFFSET = 0x0012 */
  HID_DESC_SIZE,                     /* bLength */
  HID_HID_DESCRIPTOR_TYPE,           /* bDescriptorType */
  WBVAL(0x0100), /* 1.00 */          /* bcdHID */
  0x00,                              /* bCountryCode */
  0x01,                              /* bNumDescriptors */
  HID_REPORT_DESCRIPTOR_TYPE,        /* bDescriptorType */
  WBVAL(HID_REPORT_DESC_SIZE),       /* wDescriptorLength */
/* Endpoint, HID Interrupt In */
  USB_ENDPOINT_DESC_SIZE,            /* bLength */
  USB_ENDPOINT_DESCRIPTOR_TYPE,      /* bDescriptorType */
  USB_ENDPOINT_IN(1),                /* bEndpointAddress */
  USB_ENDPOINT_TYPE_INTERRUPT,       /* bmAttributes */
  WBVAL(0x0040),                     /* wMaxPacketSize */ //OLD 0x0004
  0x40,          /* 32ms */ //OLD 0x20          /* bInterval */
/* Terminator */
  0                                  /* bLength */
};

If someone can help me :)

If you need i can send more code for help.

Thank's.
ラベル(1)
  • USB

0 件の賞賛
返信
0 返答(返信)