Content originally posted in LPCWare by studyembedded on Fri Sep 13 03:16:07 MST 2013
Yes you are right, Wouter already advised me about this, but he was talking about the example file provided by Segger. That file contains almost four different movie clips and range of fonts ....so that was quite large size. What i did is that i divided that file in two sections, first one only text animation that extracted all fonts from the said file and second for movies.
With the text animation section i have created a different project and manage to play all the animation with it. And with second part i have created this separate project where i am using a smallest possible movie clip, which can easily fit in the target board.
I just now realized that, i am adding a .lib file to my project, and that is quite huge...please check the image attached. If you can guide me how to use this .lib without adding to target build....i think it should solve my problem.
Thanks!