LPC55S16: What is the use of Product Version and Component version in commandFile.bd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S16: What is the use of Product Version and Component version in commandFile.bd

1,674 次查看
VChaudhary
Contributor III

Hi,

I am trying to use the Secure Boot option with Signed Images. I have below doubts.

What is the use of productVersion and componentVersion  in commandFile.bd, when we create SB2 file.

What I understood is they are related to customer SW versions. But how we will know which version is loaded on board?

Is there any command to get these fields?

Also, suppose I have the product version as "2.00.00" and I am trying to load SB2 with product version "1.00.00", will it work? is it down gradable?

options
{
flags = 0x4; // 0x8 encrypted + signed, 0x4 encrypted
buildNumber = 0x1;
productVersion = "1.00.00";
componentVersion = "1.00.00";
}
sources
{
inputFile = extern(0);
}
section (0)
{
erase 0x0..0x40000;
load inputFile > 0x0;
}

标签 (1)
0 项奖励
回复
4 回复数

1,652 次查看
VChaudhary
Contributor III

There are no informations available for these parameters in the "AN12283
LPC55Sxx Secure Boot". I am following the same document. Please point me to the section where they are described in detail.


Thanks

0 项奖励
回复

1,662 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend use the app note this is the informtaion available for the LPC55Sxx.

LPC55Sxx Secure Boot (nxp.com)

Best regards,
Pavel

0 项奖励
回复

1,657 次查看
VChaudhary
Contributor III

There are no informations available for these parameters in the "AN12283
LPC55Sxx Secure Boot". I am following the same document. Please point me to the section where they are described in detail.


Thanks

0 项奖励
回复

1,615 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Sorry for the late response I research more information about Secure Boot, and I find this app note may be helpful. Step by step process to prepare Secure Boot for LPC54S0xx (nxp.com)

Best regards,
Pavel

0 项奖励
回复