LPC1768 Keil Board (MCB1700) best way to switch to WiFi ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 Keil Board (MCB1700) best way to switch to WiFi ?

486 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cell85 on Tue Nov 20 08:43:26 MST 2012
Hi,

I developed a Energymeter on my MCB1700 from Keil(LPC1786). I'm using a Webinterface to visualize how much Energy my house is loosing due usage of old Washingmachines, freezers etc.
Everything works finde with the LAN on-Board.

I now want to switch to Wifi and I don't want to use a Wifi-bridge connected to the Lan-Port or something.
Is there a Wifi module which I could easily add to the board or replace with the LAN-Phy?  (Yes i want to design a new PCB)

I would appreciate your help guys.

regards
Sven
标签 (1)
0 项奖励
回复
1 回复

445 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bigkahuna on Sun Nov 25 19:21:19 MST 2012
What is the data rate you are going to need?
What is the wireless band you could use safely in your country?
What is the distance that wireless signal has to travel?
If you need something to experiment with, best to look for ZigBee board available from Sparkfun.com.  Low datarate, long distances, very easy to interface with using AT commands and cheap as any wireless boards can get.
0 项奖励
回复