Interrupt problem with write buffers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt problem with write buffers

1,288 Views
berndsirozynski
Contributor III

 

!!! never clear Interruptflags at the last line of interrupt function

 

One time more, i have found that the LPC serie has a big timing problem if clearing interrupt flags .

This problem only occures if you clear the Interrupt flag at the very last line of your interrupt function

and additional you set the compiler optimization to -O3

 

The processor needs time to clear the internal interrupt flag, but before the interrupt flag

was cleared we get a next interrupt.

 

This problem i have found in the LPC1768 and LPC1347

 

To solve the problem you need only a litte bit time or you clear the interruptflag

NOT at the very last line.

Now i always put the "DSB" instruction after clearing the interrupt flag in my functions.

 

 

In my currently project i get a I2C interrupt and the status ist 0xF8

this is an mismatch status and not described in the manual.

i think the error is an result of the internal write buffers of the CPU.

 

if i use one of the following action it works fine.

  1. a) clear interrupt flag NOT at the last line
  2. b) do an dummy operation after clearing the interrupt flag
  3. c) do not use the compiler optimization
  4. d) use an "dsb" instruction after clearing the interrupt flag

 

 

i think this behavior must described in the user manual.

0 Kudos
Reply
1 Reply

1,202 Views
soledad
NXP Employee
NXP Employee

Hi,

Thank you for your feedback, we will check this issue.

Regards

Soledad

0 Kudos
Reply