7" LCD Hardware Design for LPC54608

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

7" LCD Hardware Design for LPC54608

1,149 Views
fatihozen
Contributor IV

Hi,

I want to design my custom board and I will do somethings with lcd. Btw I chose Lpc54608. It has lcd and rtc options. I have 7" tft panel SAT070CP40D21Y0351071KTP.
You can see information about it in attachment. It is lil bit different from on board LCD panel on OM13092 eval board.
It has 40 pins. 37-40 pins are for touchscreen I think but I don't know which pins on Lpc54608 are for these 37-40 pins.
Is there any example for lcd connection and application note for this issue ?  
pastedImage_1.png 

Labels (1)
Tags (2)
0 Kudos
1 Reply

854 Views
brendonslade
NXP TechSupport
NXP TechSupport

The LPC546xx and LPC540xx boards use an LCD panel that has a built-in touch panel controller. These MCUs do not have touch panel control circuits - you would need to add one of those to your design.

0 Kudos