ı couldn't use lpc isp cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ı couldn't use lpc isp cable

2,216 Views
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by berkay on Fri Oct 31 07:10:51 MST 2014
hi, several weeks ago ı 've baught LPC isp mini programmer whose mark is waveshare, but ı didn't work. I use flash magic to send codes, when ı link isp to Comport 6 of PC and ı press BLANK CHECK button in flash magic, it gives error like Picture1 please help...  what should ı do?( ı add two Pictures which are isp and error writing)

Labels (1)
0 Kudos
Reply
8 Replies

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by berkay on Tue Nov 04 14:13:34 MST 2014
its Picture is below
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andy ESAcademy on Tue Nov 04 02:20:52 MST 2014
Yes, correct, no RS232.  :D
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Nov 04 02:13:31 MST 2014

Quote: Andy ESAcademy
...to RS232...



:quest:

And a jumper to switch 5V / 3.3V RS232  :bigsmile:
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andy ESAcademy on Tue Nov 04 02:00:57 MST 2014
Looks like the board is simply a USB to RS232 adapter. Does it also output DTR and RTS? If not then you have to manually put the target device into ISP mode. As previously mentioned, this is usually achieved by pressing reset and ISP buttons on the board (not on the adapter).

As you don't have any buttons you will need to wire them to your board yourself. Look at the Keil MCB1700 schematic on the Keil website for ideas.

Andy
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by berkay on Mon Nov 03 14:27:14 MST 2014
I checked there in flah magic everything is like your saying, there isn't any button on my isp cable, it still give me "autobaudrate fail" when ı  connect to PC's usb, probably there is one more place in flash magic to change options...
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Mon Nov 03 05:47:14 MST 2014
In Options -> Advanced Options -> Hardware Config, is "Use DTR and RTS to control RST and ISP pin" checked?

Alternatively, if the board has buttons for Reset and ISP, hold down ISP while pressing Reset, then start FlashMagic.

Are you sure everything is powered and connected correctly?
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by berkay on Sat Nov 01 02:07:40 MST 2014
I baught isp cable from aliexpress, LPC1768 from a website
0 Kudos
Reply

1,910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Oct 31 08:02:25 MST 2014

Quote: berkay
hi, several weeks ago ı 've baught LPC isp mini programmer whose mark is waveshare, but ı didn't work. I use flash magic to send codes, when ı link isp to Comport 6 of PC and ı press BLANK CHECK button in flash magic, it gives error like Picture1 please help...  what should ı do?( ı add two Pictures which are isp and error writing)



So where did you 'baught' it?  Ask them...

Which board did you connect?

Not sure which toolchain and MCU you are using. If it's LPCXpresso it could be very helpful to use debugger / programmer like LPC-Link2  :) 
0 Kudos
Reply