TWR-K40X256 Reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K40X256 Reset

跳至解决方案
1,473 次查看
billsorel
Contributor I

Hey, this is a very newbie question:  I ended up using some of the example programs to get familiar with the TWR-K40X256.  One of the tutorials i followed had the example program (flashing LED) sent to the flash memory instead of RAM.  Well, at some point something was corrupted and the program overwrote the demo program on board which has affected many things including coms.  Since it`s at the non volatile state we can`t remove it.  Is there a factory reset, such as moving a jumper on the board or a program that can reflash back to the factory demo which came onboard.  We think we have learned our lesson if we can just get back to a known working configuration.

thanks,

Bill

标记 (1)
0 项奖励
回复
1 解答
1 回复
1,359 次查看
DerekLau
Contributor IV
0 项奖励
回复