Specifications for crystal specification for MK12DX256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Specifications for crystal specification for MK12DX256

1,584 Views
DeepakK
Contributor I

Hi,

I plan to use the MK12DX256VLK5 part for a design and connect 8MHz external crystal and the 32.768KHz crystal.

I need some help in selecting the crystal/resonator for this part. In the datasheet I cannot find the required crystal specification like fundamental mode, tolerance, stability, drive specification, load specifications of the crystal. 

Does NXP have a separate white paper or design document specific to the crystal selection for this part?

0 Kudos
Reply
1 Reply

1,572 Views
Ramon_Vega
NXP TechSupport
NXP TechSupport

Hi Deepakk thanks for contact us I am glad of help,

I have some recommendations to help you

In the Datasheet https://www.nxp.com/docs/en/data-sheet/K12P80M50SF4.pdf

Please see page 27 section 6.3.2.1 Table 15. Oscillator electrical specifications, you can see some specifications and these recommendations.

1. See crystal or resonator manufacturer's recommendation

2. Cx and Cy can be provided by using either integrated capacitors or external components.

3. When low-power mode is selected, RF is integrated and must not be attached externally.

4. The EXTAL and XTAL pins should only be connected to required oscillator components and must not be connected to any other device.

Also, you can see this reference manual to get more info about connections

https://www.nxp.com/webapp/Download?colCode=K12P80M50SF4RM

Please see the page 471, 25.5 External Crystal / Resonator Connections

I hope this information help you.

Best Regards.

0 Kudos
Reply