SRAM size and location for MK64FX512VLL12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRAM size and location for MK64FX512VLL12

Jump to solution
892 Views
steve32768
Contributor II

Can someone from NXP please confirm the SRAM size and address range for the MK64FX512VLL12?

Per the datasheet, this should be 256KB, but there's conflicting information in the reference manual. The reference manual indicates a size of 256 KB, but address range of 0x1FFF_0000-0x2001_FFFF (which is only 192 KB)

See attached picture from the table in section 3.5.3.1 of the latest reference manual v.5. 

Labels (1)
0 Kudos
Reply
1 Solution
875 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.

View solution in original post

3 Replies
871 Views
steve32768
Contributor II

Thanks for the quick reply on that!

0 Kudos
Reply
882 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the MK64FX512VLL12 has 256 KB of SRAM. Still, I will escalate your remarks on the address ranges in the Reference Manual as a possible documentation error and will get back to you as soon as I receive a response.

 

Regards,

Edwin.

876 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.