Relocate Vector Table

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Relocate Vector Table

1,375件の閲覧回数
danielchai
Senior Contributor I

Hi all,

I read the manual for freescale TWR-K60N512.

It said " The Cortex-M4 assumes the RAM starts at 0x20000000 and expects the vector table to be stored in that address if the VTOR TBLBASE[29] bit is set. Because the Kinetis MCU family RAM starts at 0x1fff0000, this bit must be cleared" but it slaso said " Use the bit TBLBASE[29] to indicate the table is either on RAM with 1 or

flash with 0 ", so if in Kinetis MCU familly, I want to relocate the vector table, what should I do? Should I clear  TBLBASE[29] bit or set it?

Thanks.

-Daniel

0 件の賞賛
返信
0 返答(返信)