RESET BUTTON IS PRESSED IN WHEN POWERING THE TWR-K65F180

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RESET BUTTON IS PRESSED IN WHEN POWERING THE TWR-K65F180

550 Views
yadhukrishnanvm
Contributor III

Hi

please help.... my TWR-K65F180M board is now in bootloader mode. I am trying to update the Segger J-Link OpenSDA Firmware in my board. For that I did as per the pdf attached. But now my board is like dead. When I press the reset button RED LED lights up then YELLOW LED blinks and bootloader is shown in my computer.please help to fix it...

Original Attachment has been moved to: firmwares.zip

0 Kudos
1 Reply

389 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that FRDM-K22 has K20 processor on board, the K20 is used to implement the JLink protocol. After you download the Segger J-Link OpenSDA Firmware with the procedure:power off/Pressing Reset/Power on, dragging the "Segger J-Link OpenSDA Firmware".

After you have loaded the "Segger J-Link OpenSDA Firmware", you can power off, then power on WITHOUT precessing the Reset button, the "OpenSDA – CDC Serial Port and PEMicro/Freescale Debug App" will show up in windows device manager. You can click Computer with right mouse on PC desktop->Properties->Device Manager->Ports to check the "Open SDA..."
Hope it can help you.

BR

XiangJun Rong

0 Kudos