KL0 power consumption @ 4 mhz - 3x higher than expected.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL0 power consumption @ 4 mhz - 3x higher than expected.

739 次查看
austinappleby
Contributor I

I'm doing some basic power consumption tests on a MLK05Z32 chip and am seeing much higher power consumption than expected - with a 4 mhz system clock (fast internal reference clock, FLL disabled) and 2 mhz bus clock (OUTDIV4=1), the chip is drawing about 1.5 milliamps in a simple LED blink test. That's about 3x the draw of the competitor's chip with the same clocks & code - rather disappointing.

I'm looking for ways to reduce the power draw, but not having much luck - the application I'm evaluating the chip for will require some cycle-accurate bitbanging, so I don't think VLPR mode will work for me as the 0.8 mhz flash clock in that mode slows things down whenever there's an instruction cache miss.

Are there any other ways to reduce the power draw that I'm missing? I need deterministic 4 mhz operation, no wait states.

-Austin

标签 (1)
0 项奖励
回复
2 回复数

540 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Austin

The current consume depends on both code and hardware. Would you please help to provide your schematic then tell me where you measure current. Thanks.

Best Regards

Paul

0 项奖励
回复

540 次查看
austinappleby
Contributor I

There's no schematic to it - it's a bare MKL05Z32 chip on a breakout board with a 1 uF ceramic capacitor right next to it and I'm measuring the current into VDD through a 1 ohm resistor.

The only thing the code is doing is switching to the internal fast reference clock (IRCS 1, FCRDIV = 0, CLKS = 1, LP = 1, OUTDIV4 = 1), enabling PTB0 (SIM_SCGC5.PORTB = 1, PORTB_PCR0.MUX = 1, GPIOB_PDDR = 1), and then toggling the pin once a second.

0 项奖励
回复