I want to watch the regisiter of GPIO in nxp S32DS for arm2.2(windows ) software, but in debug mode the regisiter of GPIO do not change , Please show me, how to wath the regisiter in s32ds , thanks.
I use KEA128(S9KEAZ128AMLH) mcu and USB-ML-UNIVERSAL .
The code and the picture of regisiter as follow:
解決済! 解決策の投稿を見る。
How to watch the GPIO and other register, change or not ?? In S32DS for arm 2.2(windows)
Hi chumcu,
Some of the peripheral register are WO(Write Only), so you can not read back to check if it was changed.
Please refer to C:\NXP\S32DS_ARM_v2.2\S32DS\help\pdf\S32DS_ARM_User_Guide.pdf
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Can you tell me how to download the program to MCU with S32 Design Studio ,
and how to make sure download is successful ? Thanks.