KE02系列 PIT定时器当前值如何读取

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE02系列 PIT定时器当前值如何读取

2,315 Views
ghq926
Contributor I

KE02系列 PIT定时器当前值如何读取?

Labels (1)
0 Kudos
4 Replies

735 Views
ivadorazinova
NXP Employee
NXP Employee

Hello,

Current Timer Value Register (PIT_CVAL0)

please refer to Reference Manual for KE02 http://cache.nxp.com/files/32bit/doc/ref_manual/MKE02Z64M20SF0RM.pdf?fpsp=1&WT_TYPE=Reference%20Manu...

PIT.png

I hope this helps you.

Best Regards,

Iva

0 Kudos

735 Views
ghq926
Contributor I

这个我看了,你们的例程中找不到对Pit当前值的定义,所以我无法操作,我又不知道怎么修改

高厚清 2016 07 14

在 2016-07-13 18:11:45,"ivadorazinova" <admin@community.freescale.com> 写道:

|

|

NXP Community

|

|

KE02系列 PIT定时器当前值如何读取

reply from Iva Dorazinova in Kinetis Microcontrollers - View the full discussion

Hello,

please refer to Reference Manual for KE02 http://cache.nxp.com/files/32bit/doc/ref_manual/MKE02Z64M20SF0RM.pdf?fpsp=1&WT_TYPE=Reference%20Manu...

I hope this helps you.

Best Regards,

Iva

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Kinetis Microcontrollers by email or at NXP Community

Following KE02系列 PIT定时器当前值如何读取 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 Kudos

735 Views
ivadorazinova
NXP Employee
NXP Employee

Hello,

it should be counter = PIT_CVAL0; for reading counter of channel 0

you cannot change the value of the counter.

You can change only load value LDVAL - either while the cycle is running (it will be set after finishing current period) or if you don´t want to finish it, you have to disable channel counter, set LDVAL and enable it again.

-----------

你好,

它應該是反= PIT_CVAL0;通道0的計數器讀數

你不能改變計數器的值。

您只能更改負載值LDVAL - 週期運行的是同時完成本期後才能進行設置),或者如果你不想將完成它,你必須禁用通道計數器設置LDVAL並再次啟用它。

----------- translated by Google

I hope this helps.

Best Regards,

Iva

0 Kudos

735 Views
ghq926
Contributor I

官方提供的库文件没有定义PIT_CVALn,我是菜鸟,自己在原来的定义中加了一下,编译通过了,但读出来的数据始终为0。

这是我pit.h中修改的一条

这是主函数中读取定时器当前值的部分,请教问题出在哪?有没有更新的库文件?我主要目的是测量交流点的周期,(最终目的是交流同步采样)。有更好的方法吗?

在 2016-07-19 21:40:11,"ivadorazinova" <admin@community.freescale.com> 写道:

|

|

NXP Community

|

|

KE02系列 PIT定时器当前值如何读取

reply from Iva Dorazinova in Kinetis Microcontrollers - View the full discussion

Hello,

it should be counter = PIT_CVAL0; for reading counter of channel 0

you cannot change the value of the counter.

You can change only load valueLDVAL - either while the cycle is running (it will be set after finishing current period) or if you don´t want to finish it, you have to disable channel counter, set LDVAL and enable it again.

0 Kudos