K60 (mask 4N22D) reset_b pin remians low after power on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 (mask 4N22D) reset_b pin remians low after power on

Jump to solution
1,002 Views
stathis
Contributor I

RESET pin of a custom prototype board with a K60 remains always low.

We have try to slow down the power up rise time according to community suggestions

regarding similar problem but with no result.

Any other suggestions ?

0 Kudos
1 Solution
625 Views
rogerfl
Contributor III

I had this problem and solved it by making sure the EzPort pin was pulled high.  Discussed here: https://community.freescale.com/thread/312644

View solution in original post

0 Kudos
4 Replies
626 Views
rogerfl
Contributor III

I had this problem and solved it by making sure the EzPort pin was pulled high.  Discussed here: https://community.freescale.com/thread/312644

0 Kudos
625 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Turn off the board system.

2. Assert the reset pin and hold it asserted for the remainder of the process.

3. Power on the board

4. Start a debug session and as soon it is starting release the reset button. This will force the debug session to enter.

For further reset connection recommendations refer to the Kinetis Quick Reference User guide: http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1 Section "2.1.3.4.1 RESET_b and NMI_b" .

Hope this helps.

625 Views
hectorsanchez
Contributor IV

Hi Stathis,

If your flash memory is blank(No projects programmed), try to program it with an example or a custom project

Keep me informed if this fixed your issue

Best Regards,

Héctor Sánchez

0 Kudos
625 Views
stathis
Contributor I

Dear Hector,

thank you for your fast reply.

The flash is empty but the problem is that with low reset pin I can not communicate with it using PE multilink universal.

So I can not program anything on it.

Best regards

Stathis

0 Kudos