Hi: Can anyone tell me where I'm wrong in write internal flash application?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi: Can anyone tell me where I'm wrong in write internal flash application?

1,946 次查看
alessiodemarchi
Contributor I

Hi everybody.

I'm try to use the last sector of flash (S9KEAZN8 micro) as a simple eeprom (I have to save some trimming value for my application). I use IAR WorkBench as development tool.

This is the code:

void waitForCommandExecute()
{
unsigned char statVal;

  do {
    statVal = FTMRE_FSTAT;
    statVal &= FTMRE_FSTAT_CCIF_MASK;
  } while (statVal == 0);
}

....

/* The next row is where the program stop working */

  if ((FTMRE_FCLKDIV & FTMRE_FCLKDIV_FDIVLD_MASK) != FTMRE_FCLKDIV_FDIVLD_MASK)
  {
    waitForCommandExecute();
    FTMRE_FCLKDIV = ((configBUS_CLOCK_HZ / 1000 + 399U) / 1000U - 1U);
    FTMRE_FCLKDIV |= FTMRE_FCLKDIV_FDIVLCK_MASK;
  }

  if ((FTMRE_FSTAT & FTMRE_FSTAT_ACCERR_MASK) != 0)
    FTMRE_FSTAT |= FTMRE_FSTAT_ACCERR_MASK;
  if ((FTMRE_FSTAT & FTMRE_FSTAT_FPVIOL_MASK) != 0)
    FTMRE_FSTAT |= FTMRE_FSTAT_FPVIOL_MASK;

      // EEPROM/Flash erase
      FTMRE_FCCOBIX = 0x00;
      FTMRE_FCCOBHI = 0x0a; // sector Erase
      FTMRE_FCCOBLO = 0x00;
      FTMRE_FCCOBIX = 0x01;
      FTMRE_FCCOBHI = (u8_t)(BASE_FLASH_EEPROMADDRESS >> 8);
      FTMRE_FCCOBLO = (u8_t)(BASE_FLASH_EEPROMADDRESS & 0xff);

      FTMRE_FSTAT |= FTMRE_FSTAT_CCIF_MASK;
      waitForCommandExecute();

....

But when I execute the code step by step the Ide freeze with a message program of flash ...

I don't know what happens. Can anyone help me?

Thanks

0 项奖励
回复
4 回复数

1,670 次查看
alessiodemarchi
Contributor I

Thank you for the answer.

Now I'm try to execute code from ram. I will return my result probably tomorrow.

0 项奖励
回复

1,670 次查看
alessiodemarchi
Contributor I

The code should act as flash sector erase, but the problem is the same as for the flash write.

0 项奖励
回复

1,670 次查看
mjbcswitzerland
Specialist V

Hi Alessio

      FTMRE_FSTAT |= FTMRE_FSTAT_CCIF_MASK;
      waitForCommandExecute();

must be executed from SRAM and not from Flash - it will immediately fail if executed in Flash since the Flash becomes unreadable while it is being erased. Also one usually protects the call from interrupts since an interrupt will usually cause Flash to be accessed and so a failure too.

To save time, this is available in the uTasker KEA project, which is available as open source at
http://www.utasker.com/forum/index.php?topic=1721.msg7086#msg7086

Its flash driver is compatible with all Flash and EEPROM in KE, KEA, KL, K etc. parts and includes Flash emulation to identify issues before they get to the HW (with fail-safe parameter system in Flash/EEPROM emulation).

Regards

Mark

Professional support for Kinetis: http://www.utasker.com/index.html
Remote desktop one-on-one coaching: http://www.utasker.com/services.html
Getting started to expert videos: https://www.youtube.com/results?search_query=utasker+shorts

0 项奖励
回复

1,670 次查看
alessiodemarchi
Contributor I

Hi.

I try to execute the code from FLASH but with interrupt disabled and the code is running well.

Tomorrow I try a long test.

Thanks a lot

0 项奖励
回复