Freescale/NXP_Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale/NXP_Kinetis

2,232件の閲覧回数
piotrmazur
Contributor I

Good afternoon,

We have made a transceiver project ( and got it ready for production lots of

months ago) based on TI company's product CC2538. Unfortunately, up till

the present moment we haven't been given the access to stack_u ZigBee IP

SE2.0 by TI. We would like to accomplish the project by replacing wireless

MCU from TI by the product available in Freescale/NXP. Having in mind

mentioned above, we'd like to ask you for the following information :

1. If NXP will continue to produce and further sell of MCU Kinetis

series?

2. Since when stack ZigBee IP for MKW24D512V was made available by

Freescale/NXP? ( was it also for Kinetis series products?)

3. Can Freescale/NXP offer us any Evaluation Boards, Demo Board & Kits

( MKW2x on board) with working stack ZigBee IP?

Above questions were asked based on the information contained in folders

describing MCU Kinetis series: "The Kinetis KW2xD wireless MCU provides a

low-power, compact integrated device for smart energy 1.x, home automation,

healthcare, and RF4CE, as well as the ZigBee IP network stack and the smart

energy 2.0 application profile.

With kind regars,

Piotr Mazur

e-mail: [email protected]

tel.+48 34 3770300

kom. 500 195505

Cerber Property Spółka z o.o. S.K.A

ul. Mirowska 157

42-200 Częstochowa

NIP: 949-219-12-97

0 件の賞賛
返信
2 返答(返信)

1,737件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

First, welcome to NXP! :smileyhappy:

Please let me answer to your question below:

1.       If NXP will continue to produce and further sell of  MCU Kinetis

series?

>> Yes, See Product Longevity: NXP (formerly Freescal&#10|NXP .

2.       Since when stack ZigBee IP for MKW24D512V was made available by

Freescale/NXP? ( was it also for Kinetis series products?)

>>Yes, you can download Kinetis BeeStack ZigBee Protocol Stack

from the link below:

https://www.nxp.com/webapp/Download?colCode=KINETIS-BEESTACK&appType=license&location=null&Parent_no...

3.       Can Freescale/NXP offer us any Evaluation Boards, Demo Board & Kits

( MKW2x on board) with working stack ZigBee IP?

We provide the FRDM-KW24D512 fredom board for evaluation.

NXP Freedom Development Platform for Kinetis |NXP

1,737件の閲覧回数
piotrmazur
Contributor I

Thank you very much for reply.

1.Could you please inform me since when ZigBee IP SE2.0 is present in KinetisBeeStack ZigBee Protocol Stack ? Can Freescale/NXP precise the year and month of making ZigBee IP 2.0 accessible for own customers? This is an essential information for us to make  decision about replacing TI hardware with the solution being currently offered by NXP.

  2.Is NXP planning, in the nearest future, to use next version of ZigBee 3.0 for own Kinetis series?

0 件の賞賛
返信