FRDM-KE04Z Bootloader error in Win8.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KE04Z Bootloader error in Win8.1

1,183件の閲覧回数
jonathanm
Contributor I

Hi,

I'm working with a Freedom Board with this HW Info:

Board Name is: FRDM-KE04Z

MicroBoot Kernel Version is: 1.05

Bootloader Version is: 1.10

Installed Application: PEMicro FRDM-KE04Z Mass Storage/Debug App

Application Version is: 1.14

In Win7 (64 bits), it works fine loading SDA Applications and Precompiled demos with the MSD.

However, in Win8, once I connect the board, the OpenSDA Status Led gives an error (2 seconds off followed by 8 rapid on/off blinks), and it does not go out of Bootloader mode. The only way I've found to correct this is to connect it again in Win7 and load the SDA file again.

How could I solve this problem in the Win8.1 OS?

Thanks for your help.

0 件の賞賛
返信
1 返信

1,056件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jonathan,

To provide the fastest possible support I want to point you to a similar question which has been answered on our Freescale community. Please refer to Re: hello everyone, recently i have bought frdm kl-46z board. but i got a problem loading driver for...  to view the details.

Wish it helps.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信