makefile:136: recipe for target 'HEXIWEAR_MK64.elf' failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

makefile:136: recipe for target 'HEXIWEAR_MK64.elf' failed

3,719 Views
ice_hevean
Contributor I

Hi everyone,

  I am new with KDS and I tried to use KDS to perform firmware changes on a IoT device, Hexwear, I have encountered the error of makefile:136: recipe for target 'HEXIWEAR_MK64.elf' failed once I build the source file of the firmware from source code of the firmware.

pastedImage_2.png

Any method to fix? 

Thank you so much!!!!

Labels (1)
0 Kudos
Reply
2 Replies

2,287 Views
tlraghavendra
Contributor I

Hi,

i am facing same issue. in library paths i can see Pedomenter. but still got same error

Please advice.

 

Raghavendra

0 Kudos
Reply

3,553 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Frances,

 

This stack is not NXP proprietary so for more information I will suggest to contact Hexiwear for this, but the log file mention that a file wasn't found, the path that mention I think the libPedometerLib.a. Maybe in the library paths (right click -> properties -> C/C++ General -> Paths and Symbols) the right path for the library isn't added.

 

Best Regards,

Alexis Andalon

0 Kudos
Reply