Hi,
I was trying to integrate FreeScale safety library for CM0+ to my Freedom KL25Z development board.
As the library is provided in ".a" format with associated headers, I followed the necessary steps as described in below:
Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse
But when Building the project I receive an error that the Code warrior is not able to locate/ find the library. Please see attached files for error details.
What I am doing wrong ?
Hi,
I also wants to integrate the same library in my Codewarrior project. But the library is compiled for IAR compiler.
Can you please help me in this regard?
I shall be very much thankful to you for this. PS: I'm a bit new into this field, sorry for dumb question.
Best Regards
Taimur
Hi Erich,
Thanks for the quick reply. I wants to use NXP safety library in my codewarrior project. I'm using Kinetis K10 with cortex M4. Is there any work around? Can I compile the library manually?
Best Regards
Taimur
Hi Erich,
yes, I think I do have the library source file. Can you please provide me the necessarg steps to built my own library?
I have been through this post
Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse
but not able to built the library.
One of my questios is where should I add the library sources, after creating the library project?
and the library contain couple of .S files, and when I compile the sources, I gets compilation errors.
Thanks for your help.
You can add the sources like to any other project, that does not matter. Make sure you include with the -I (include header file path) the folder where you have your sources.
As for .S (assembly) files: keep in mind that IAR mostly uses a different syntax than the GNU assembler. So if they are not in the GNU format, you have to port the assembly files.
Erich