Kinetis Design Studio  Version: 3.0.0 crashes when I try to upload code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio  Version: 3.0.0 crashes when I try to upload code

1,121件の閲覧回数
gibson486
Contributor I

I get this error when I try to upload code to a FRDM-K22.

 

An internal error occurred during: "Launching demo_Debug_OpenOCD".

ilg.gnuarmeclipse.debug.gdbjtag.dsf.GnuArmServicesFactory.<init>(Ljava/lang/String;Ljava/lang/String;)V

ラベル(1)
0 件の賞賛
返信
1 返信

1,041件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Andrew,

It seems to me that you have done an update with newer GNU ARM Eclipse debug plugins? If so, there is a know issue with these plugins affecting OpenOCD and Segger J-Link.

See this thread Unable to Debug after KDS Update  which has a workaround attached to it.

I hope this helps,

Erich

0 件の賞賛
返信