ETA on full integration of MQX with KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETA on full integration of MQX with KDS

826 Views
intractablesubt
Contributor III

Can you give a more specific ETA on when the full integration of MQX with KDS will be complete? As I showed in my last reply in a previous post KDS 1.1.0 adding MQX component using processor expert fails build, the current status is that MQX is incompatible with Processor Expert, at least as far as I can tell. I'm about to start a major development and would rather wait for the fully integrated package if it's imminent.

Labels (1)
0 Kudos
2 Replies

435 Views
dereksnell
NXP Employee
NXP Employee

Hi William,

The latest MQX release v4.1.1 has support for Kinetis Design Studio (KDS) toolchain.  But your issue is specific to the MQX for KSDK release.  The current v1.0.0 Beta release for this available, see Beta version of MQX RTOS for Kinetis SDK - Now Available.  This does have current support for Processor Expert, both with KDS or using the stand-alone Processor Expert Driver Suite for other toolchains.  See the tutorial for using MQX for KSDK with Processor Expert.  The production release for MQX for KSDK v1.1.0 is planned for Decemeber, like David said.

Thanks

0 Kudos

435 Views
DavidS
NXP Employee
NXP Employee

Hi William,

The last update I saw had the KDS/KSDK+MQX+PE support for mid-December, 2014.

Regards,

David

0 Kudos