About Relative paths.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About Relative paths.

3,729 次查看
TsuyoshiSugiyama
Contributor II

I want to make the path of the Gui Guider source a relative path.

Currently, the image path is absolute.

When sharing source code with others, absolute paths are difficult to compare.

Is it possible to make the source code in the .guiguider file a relative path?

 

7 回复数

2,519 次查看
cjssi
Contributor II

Hello,

It is a year and a half since this question was asked, and using GUI Guider 1.7.2 under Windows, I am seeing the same behavior. Specifically, if I manually edit the .guiguider file to have only relative paths, they resolve correctly, but GUI Guider saves the absolute paths back to the .guiguider file rather than keeping them in memory only. This means that I have to manually edit the file every time I want to merge my code back to the master branch, which is suboptimal to say the least as well as rather surprising: it is not expected behavior that opening a file results in it being changed.

I would like to request that paths in the .guiguider file be retained as-is after import, save, and generate operations. This will allow version control to work properly and will not force developers to manually edit before every merge.

Thank you.

0 项奖励
回复

2,462 次查看
WenbinYuan
NXP Employee
NXP Employee

Hello @cjssi,

 

Sorry for the inconvenience you have experienced.

 

The feature for relative paths has been added to the functionality list for V 1.9.0, and we hope that upon its official release, it will improve your user experience.

 

BR,

Wenbin

3,710 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @TsuyoshiSugiyama 

GUI Guider current version doesn't have feature of using relative path.

I have logged it as feature request to GUI development team just now. 

Thanks for bringing the problem to our attention.

Have a nice day,

Jun Zhang

3,320 次查看
josephchen
Contributor III

Hi @ZhangJennie 

Is there any update on the issue?

0 项奖励
回复

3,290 次查看
WenbinYuan
NXP Employee
NXP Employee

Hi @josephchen,

 

Now the paths in .guiguider file are still using absolute path, but it will update automatically when another user import this project into GUI Guider.

And all images imported into project will be copied  to 'import/image', so the absolute paths will not cause any issue when sharing project between GUI Guider users. 

 

Best Regards,

Wenbin

0 项奖励
回复

3,284 次查看
josephchen
Contributor III

Hi @WenbinYuan,

 

For a team using Git to manage code, using relative paths in .guiguider file is more appropriate.

 

Kind Regards,

Joseph Chen

0 项奖励
回复

3,282 次查看
WenbinYuan
NXP Employee
NXP Employee

Hi @josephchen,

 

Thanks for your feedback, we will consider the Git usage and try to improve the GUI Guider.

 

Best Regards,

Wenbin