what is the highest variable frequency FreeMaster supported when using DAP connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the highest variable frequency FreeMaster supported when using DAP connection

1,813 Views
momomomo
Contributor I

When I use FreeMaster, when DAP connects to the highest speed and collects variables at 200kHz, the displayed waveform always has problems, while low-frequency ones are fine. Why is this? The speed is always set to the fastest

0 Kudos
Reply
1 Reply

1,800 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

it is a simple question, but it is not so easy to answer. Our experiments show that with CMSIS-DAP at default 1MHz, the maximum is around 2k of 32bit samples per second. Increasing the DAP clock speed does not always bring the desired performance increase. With JLink it may reach up to 10k samples. 

The fastest communication interface is a USB CDC port implemented by USB-enabled NXP devices (see fmstr_usb_cdc demo) or UDP communication for NXP devices with Ethernet interface.

Anyway, FreeMASTER was not really intended to be used as a high speed live recorder. In order to capture transitions at very high speed, use a FreeMASTER Recorder feature - which runs at the MCU side and uses on-chip memory for recording. With FreeMASTER Recorder, you should be able to record data around 100kHz rate.

Regards,
Michal

0 Kudos
Reply