Freemaster Protocol on CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster Protocol on CAN

Jump to solution
2,138 Views
nxf64554
NXP Employee
NXP Employee

Hi, Is there any documentation about how Freemaster protocol is encoded (i.e. in CAN messages)?

I am trying to understand the low level of the communication driver code so I might be able to modify it for a specific application.

Thanks!

1 Solution
2,042 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Weilin Cao,

the FreeMASTER-over-CAN protocol uses the same command/response format as a "native" Serial protocol. The payload is split to 7-byte chunks and is transmitted over a simple CAN signalling protocol. I'm attaching a white paper which describes general concepts of both Serial protocol and also the CAN transport.

Best regards,

Michal

View solution in original post

2 Replies
2,043 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Weilin Cao,

the FreeMASTER-over-CAN protocol uses the same command/response format as a "native" Serial protocol. The payload is split to 7-byte chunks and is transmitted over a simple CAN signalling protocol. I'm attaching a white paper which describes general concepts of both Serial protocol and also the CAN transport.

Best regards,

Michal

2,041 Views
nxf64554
NXP Employee
NXP Employee

Thanks that is exactly what I am looking for!

0 Kudos
Reply