Hello Luca,
yes as discussed in other two posts in this forum, the FreeMASTER Edge browser component crashes after a recent Windows/Edge update deployed by Microsoft. This issue affects all FreeMASTER 3.2.x versions with Edge support.
As Edge is the default component used to render the Welcome page, the FreeMASTER crashes as soon as you run it. When you run FreeMASTER by opening a project which uses IE or CEF engine to render HTML, then the FreeMASTER works normally (until you do File/New).
Another workaround is to rename the "c:\NXP\FreeMASTER 3.2\FreeMASTER\html" to html.bak to prevent the Welcome page to load. But still using Edge engine to render project-specific content may have issues.
We have identified the root cause of the issue and we are now working on hotfix release. This should be out during the next week - early Sep/2023.
Thanks for staying with us,
Michal