stack corruption in jffs2 using SLUB (2.6.25 kernel) on cf5475

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

stack corruption in jffs2 using SLUB (2.6.25 kernel) on cf5475

2,244件の閲覧回数
Plasmasam
Contributor I
While trying to get the new 2.6.25 ltib working we came across very strange things while mounting larger
(>20MB) jffs2 partitions on NOR-Flash. Our configuration is very similar to EVB board, the main difference
is 128MB DDR and 32MB NOR-Flash. We got u-boot as well as kernel running and everything is fine when working on nfs root.

When trying to mount a jffs2 partition we've got bad page and crash deep in
jffs2/malloc.c jffs2_alloc_inode_cache() where kmem_cache_alloc() is used.
More detailed investigation shows that this is only a follow-up symptom, things get mixed-up already when calling kmalloc() in jffs2/build.c function do_mount_fs().

What is interesting, this crash occurs only if:
- SLUB allocator is used
- Partition is larger than ~20MB (w/ 128k erase block) which results to kmalloc of more than 8k (>single page)
- "compile kernel with frame pointers" is off in kernel config

Tracing down the issue we found that kmalloc() in do_mount_fs() returns a totally invalid pointer. But deeper in kmalloc code everything looks ok down to mm/page_alloc.c __get_free_pages(), only the returned pointer is mixed-up somewhere on its way. Looking at the stack content at various points shows that stack pointer is not getting back where it was before kmalloc() call, it is off by -0x10.
I attached a sample stack log with some comments to document this.

We are now really concerned about using the new kernel / slub allocator.

Could someone look deeper into this ?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,410件の閲覧回数
Plasmasam
Contributor I
Doing some further investigation shows that this might not be related to jffs2 at all but that kmalloc is here generally broken with SLUB if size > PAGE_SIZE ! (I have put the same call to kmalloc outside of jffs2 code)
0 件の賞賛
返信

1,410件の閲覧回数
J2MEJediMaster
Specialist I
I checked with an engineer here and you may have found a bug. To have it handled properly, you need to submit a Service Request on it. To enter a service request to Freescale, click here.
 
---Tom
0 件の賞賛
返信