Place MC68332 in high impedance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Place MC68332 in high impedance

1,592 Views
chriscrde
Contributor I
Hello,
I'm developping a board test in boundary scan and i need to place an MC68332 in high impedance in order to test adress and data bus of the board.
I think that i have to use the TSC pin but I don't know how to use it. The document M68331/332TUT/D says that :

Driving this pin to approximately 1.6 times causes the MCU to place all output drivers in a high-impedance state, isolating the MCU from the rest of the system.

But it doesn't work.

Can you say me how to do ?

Thanks

 

Labels (1)
0 Kudos
Reply
1 Reply

333 Views
macl
Senior Contributor I
Hi,
 The TSC signal must remain asserted (1.6*VDD) for approximately ten clock cycles in order for drivers to change state.  This is 8V for 5V VDD.  Just don't go over 9V.
 
Thanks,
Mac
0 Kudos
Reply