MCF5232CVM150 and MC9S08GB60A Ultrasonic Cleaning?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5232CVM150 and MC9S08GB60A Ultrasonic Cleaning?

529 次查看
RussellPead
Contributor II

MCF5232CVM150 and MC9S08GB60A.

 

  1. Can these devices be Ultrasonic clean?
  2. Our CM is using SANHO-Ultrasonic Engineering Ltd equipment, is this acceptable?
  3. Our CM is using a single frequency (28KHz), will this frequency causes a latent damage to the wire bond inside the device?
  4. If 28KHz does causes damage to the device, what is the right frequency to use? (alternating/variable frequency) 
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

392 次查看
miduo
NXP Employee
NXP Employee

Hi,

Please be note that : NXP don't test or qualify devices for ultrasonic cleaning since almost no customers use this cleaining method. The most commond cleaning method is to use high pressure water based spray wash which our devices have no problems with.  Ultrasonic cleaning has a potential for damaging various devices on a PCB assembly.

Best Regards,

Fang

0 项奖励
回复