LS1012A with LSDK 17.06

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A with LSDK 17.06

821 Views
justinjonas
Contributor III

Does the LSDK 17.06 software work with the LS1012A? If so has the PFE software changed?

Tags (1)
0 Kudos
1 Reply

517 Views
Pavel
NXP Employee
NXP Employee

There are "LSDK" and "SDK". These are different things.
The SDK is the yocto-based package we have been supplying for some time; the latest release is 2.0-1703. This supports LS1012A. Please see:
http://www.nxp.com/products/developer-resources/run-time-software/linux-sdk/linux-sdk-for-qoriq-proc...

LSDK isn't yocto-based. It has just had a 1706 release, which adds support for a larger number of devices, but notably does not yet include support for LS1012A. Please see:
http://www.nxp.com/products/developer-resources/run-time-software/linux-sdk/layerscape-software-deve...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos