Compiler bug when setting "Parameter Passing" option to "Compact".

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler bug when setting "Parameter Passing" option to "Compact".

2,318件の閲覧回数
Claude_Sylvain
Contributor I
Hello,
 
I currently work on a project that use MCF52223 MCU.
 
At the begining of the project, the "Parameter Passing" option was set to "Compact", and all was working fine (the target was running well).
 
Later on, after some code was added to the project, and compiled successfully; when I start the target, an exception error occur, telling that the MCU was out of control.
After searching a long time for a possible coding error without success, I finally found that the compiler generate bad code on some special case :smileymad:
The only mean I found to get rid of that problem is to set the "Parameter Passing" option to "Standard".
 
That bug was there in CodeWarrior V6.3, and is still there in CodeWarrior V6.4.
 
Since, this bug can be avoided by setting the "Parameter Passing" option to "Standard",  it is not very anoying :smileyhappy:
 
But, I am wondering if it is possible to submit a bug report, and how to proceed.
Do I have to contact my local dealer, or can I submit it directly to Freescale?
 
 
Claude Sylvain
Electro-Technica inc.
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

498件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hello,
I suggest you submit a bug report (support@freescale.com). Best with a short reproducible case (if possible). That way the compiler engineers could have a look and get it fixed.

Thanks!
Erich
0 件の賞賛
返信

498件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hello,
there is an even better way than I mentioned in my previous post to submit a bug report:
Click here to submit a service request.

Erich
0 件の賞賛
返信

498件の閲覧回数
Claude_Sylvain
Contributor I
Hello Erich,
 
I tracked down the bug, and sent a little project that show the bug to the service request of Freescale.
 
 
Thank you for your help.
 
Claude.
Electro-Technica inc.
 
0 件の賞賛
返信