Warning : C12056 SP debug info incorrect because of optimization or inline assembler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Warning : C12056 SP debug info incorrect because of optimization or inline assembler

2,260 Views
rayhall
Contributor V

I am getting the C12056 warning for the following function.The fuction works perfectly. Can someone explain what is wrong ?

 

int16_t Interpolate3D(uint16_t *table, uint8_t axisXCnt, uint8_t axisYCnt, uint16_t xAxis, uint16_t yAxis)
{
    uint8_t x, y;
    int16_t Q11, Q12, Q21, Q22;
    int32_t val1, val2;
    int32_t interpVal;
    float ratioX, ratioY;

 

    x = 0;
    y = 0;
    Q11 = 0;    // x-axis minimum interpolation value
    Q12 = 0;    // x-axis maximum interpolation value
    Q21 = 0;
    Q22 = 0;


    if (xAxis <= table[0] || xAxis >= table[axisXCnt - 1])
    {
        if (xAxis <= table[0])    // less than minimum x value in table?
        {
            Q11 = table[0];
            Q12 = table[1];
            xAxis = Q11;    // adjust to minimum value
            x = 0;            // AG just to make sure
        }
        if (xAxis >= table[axisXCnt - 1])    // greater than maximum x value in table?
        {
            Q11 = table[axisXCnt - 2];
            Q12 = table[axisXCnt - 1];
            xAxis = Q12;        // adjust to maximum value
            x = axisXCnt - 2;    // AG addition, index to last but one element of x axis
        }
    }
    else    // locate table entries that surround xAxis value
    {
        for (x = 0; x < axisXCnt; x++)
        {
            if (table[x] <= xAxis && xAxis < table[x + 1])
            {
                Q11 = table[x];
                Q12 = table[x + 1];
                break;
            }
        }
    }
    ratioX = (float)(xAxis - Q11) / (float)(Q12 - Q11);


    if ((yAxis <= table[axisXCnt]) || (yAxis >= table[(axisXCnt << 1) - 1]))
    {
        if (yAxis <= table[axisXCnt])
        {
            Q11 = table[axisXCnt];
            Q12 = table[axisXCnt + 1];
            yAxis = Q11;
            y = 0;        // AG just to make sure
        }
        else
        {
            Q11 = table[(axisXCnt << 1) - 2];
            Q12 = table[(axisXCnt << 1) - 1];
            yAxis = Q12;
            y = axisYCnt - 2;
        }
    }
    else
    {
        for (y = 0; y < axisYCnt; y++)    // AG comment - should be axisYCnt-1 but probably works as-is
        {
            if ((table[y + axisXCnt] <= yAxis) && (yAxis <= table[y + axisXCnt + 1]))
            {
                Q11 = table[y + axisXCnt];
                Q12 = table[y + axisXCnt + 1];
                break;
            }
        }
    }
    y += 2;        // offset so that index points to correct real data row

 

    ratioY = (float)(yAxis - Q11) / (float)(Q12 - Q11);
    Q11 = table[x + (axisXCnt * y)];
    Q12 = table[x + (axisXCnt * y) + 1];

 

    Q21 = table[x + (axisXCnt * (y + 1))];
    Q22 = table[x + (axisXCnt * (y + 1)) + 1];

 

    val1 = Q11 + (ratioX * (Q12 - Q11));
    val2 = Q21 + (ratioX * (Q22 - Q21));

 

    interpVal = val1 + (ratioY * (val2 - val1));


    return (int16_t)interpVal;
}

 

Ray.

Labels (1)
0 Kudos
Reply
1 Reply

1,878 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ray.

I just attached document about C12056, please check if you can sort out your problem with it.

if can't please provide your demo project, we need reproduce it and will work on it directly.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply