The USB-Jtag download quesiton with CW10.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The USB-Jtag download quesiton with CW10.6

585 次查看
yongyan
Contributor II

The question I've meet is that I used the TWR-56F8400 board's OSBDM to download the program to my MC56F84789 chip,but it's alaways failed. When I cut the main circuit'sinta power and only link the TWR_56F8400's USB port to my computer,link the TWR-56F8400's JTAG port to the main circuit's JTAG port , the code can be downloaded to the main circuit 'MC56F84789 chip .However,when I turn on the main circuit's power.It's always failed to download.The CodeWarrior's intarface shows that the chip is secured. pastedImage_1.pngWhen I click the "yes" button,It shows……pastedImage_1.png.

When I click the retry,it still don't work and popup the same window.

It really bother me a lot.I'm looking forward to your help.

Best Regards,

Yong Yan

0 项奖励
回复
1 回复

484 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Yong.

This is the same question as

https://community.nxp.com/message/943622 

Please refer above link for answer. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复