Issue with Reserved range overlap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with Reserved range overlap

Jump to solution
558 Views
MWMinor
Contributor V

Hi

 

I have migrated my CW V10.6 tools to a new laptop. When I imported a design (Coldfire MCF51JM128 product design) from my old laptop ( which also was running V10.6) I successfully compiled the design but am failing to programme the devices on my custom board. The board was working with the old laptop, but now I get an error;

58958_58958.pngpastedImage_0.png

I'm not sure where the configuration file is stored/generated, can anyone help me please.

 

Thanks

 

Ken

Labels (1)
0 Kudos
Reply
1 Solution
426 Views
BlackNight
NXP Employee
NXP Employee

The memory configuration file is usually stored inside <project>\Project_Settings\Debugger\*.mem

Erich

View solution in original post

0 Kudos
Reply
2 Replies
427 Views
BlackNight
NXP Employee
NXP Employee

The memory configuration file is usually stored inside <project>\Project_Settings\Debugger\*.mem

Erich

0 Kudos
Reply
426 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ken,

from the error screenshot, the error is on the memory configuration file. please refer with attached video to check your memory configuration file setting.

I also attach MCF51JM128.mem from my side.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply