I am using the 9s12p128 and codewarrior ver 5.2, why no load the file *.abs in debugger with PEmicre corvus ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am using the 9s12p128 and codewarrior ver 5.2, why no load the file *.abs in debugger with PEmicre corvus ?

1,286件の閲覧回数
hectorleal
Contributor II

Is all

0 件の賞賛
返信
6 返答(返信)

1,060件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

could you please upload a problem screenshot?

Thanks,


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,061件の閲覧回数
hectorleal
Contributor II

This the screenshot

I beginning in Codewarrior, Cyclonepro and have Codewarrior ver. special

5.2 and Cyclonepro Corvus

The microcntroller is 9S12P128 for liquid sensor and scrren 20X4

Alphanumerics

Atte.

Héctor Leal

P.D. I am sorry mi bad english

2018-02-22 7:02 GMT-06:00 ZhangJennie <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: I am using the 9s12p128 and codewarrior ver 5.2, why no load the file

*.abs in debugger with PEmicre corvus ?

reply from ZhangJennie

<https://community.nxp.com/people/ZhangJennie?et=watches.email.thread> in *CodeWarrior

for MCU* - View the full discussion

<https://community.nxp.com/message/989153?commentID=989153&et=watches.email.thread#comment-989153>

0 件の賞賛
返信

1,061件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hector

I would suggest you go to debugger menu "File", "Configuration...", force your code stop at a function after load:

pastedImage_1.png

Can this help you? If not, please upload your demo project, I have to check it directly.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,061件の閲覧回数
hectorleal
Contributor II

​​​​Hello Jennie:

In this mail is the project and screens

Tanks

0 件の賞賛
返信

1,061件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hector,

I didn't see your project, can you send it?

Thanks.

Jennie Zhang

0 件の賞賛
返信

1,061件の閲覧回数
hectorleal
Contributor II

​​​​Hello Jennie:

In this mail is the project ​

Project_1.rar

<https://drive.google.com/file/d/1SvbJrB_P0bHNznorXqJWiXNDZpOpKUDW/view?usp=drive_web>

Tanks

2018-02-27 0:28 GMT-06:00 ZhangJennie <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: I am using the 9s12p128 and codewarrior ver 5.2, why no load the file

*.abs in debugger with PEmicre corvus ?

reply from ZhangJennie

<https://community.nxp.com/people/ZhangJennie?et=watches.email.thread> in *CodeWarrior

for MCU* - View the full discussion

<https://community.nxp.com/message/990476?commentID=990476&et=watches.email.thread#comment-990476>

0 件の賞賛
返信