CodeWarrior as a simple ICE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior as a simple ICE?

跳至解决方案
1,698 次查看
stephenhanka
Contributor I

I have never used CodeWarrior but I have a need for it.  I have CodeWarrior 10.1.1 targeting a P2040 running Linux with a USB JTAG TAP installed.  The board is occasionally locks up under certain conditions.  What I want to do is boot the board from flash wait for it to lock up, then break in with CodeWarrior and dump the registers, most importantly the program counter.

 

I don't see anything in the user documentation on how to do this.  I don't need to develop and download code.  I only want to dump the registers when the board locks up.  Can someone tell me if there is a simple way to do this?

标签 (1)
0 项奖励
回复
1 解答
1,595 次查看
BlackNight
NXP Employee
NXP Employee

I have not used a P2040 with Linux, but I think this article might help you:

http://mcuoneclipse.com/2012/10/10/attach-connect-download/

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,596 次查看
BlackNight
NXP Employee
NXP Employee

I have not used a P2040 with Linux, but I think this article might help you:

http://mcuoneclipse.com/2012/10/10/attach-connect-download/

0 项奖励
回复