Hello,
ok, I think I have now the same issue you are seeing :smileysad:.
Interestingly it fails to connect both with the onboard P&E Multilink and an external one (I have soldered the BDM header on my board) with MCU10.2 (did not try with 10.1).
I tried to connect to the board using MCU6.3 (the non eclipse version) using the onboard P&E, and this failed too.
But when I did it with an external Multilink, then it worked!?!
It looks to me that there is some kind of difference in the P&E DLL/firmware.
Do you have an external USB Multilink with MCU6.3 you could try?
I'll see if I can reproduce things in the office on Monday, so I can report this to P&E.
BK